Archiving allows you to create a copy of selected data on another storage device, whether it be an exacqVision S-series storage server, a user provided storage server, exacqVision Cloud Drive, an Amazon S3 account, or Wasabi S3 account. This video explains how to create a new archiving profile, establish the archiving task, then schedule the… Continue reading Archiving
Tag: Cloud Drive
Cloud drive relies on the bit rate, not the quality when archiving the cameras.
Description When choosing a subscription for a camera on a cloud drive, it relies on the bitrate, not the quality. Example: You are selecting a 4K subscription for an Illustra Flex2 4K Dome camera on the could drive.
Unable to Find MAC Address During Exacq Cloud Drive Archiving Setup
Description After performing all steps found in Knowledge Base Article #7697 up to Step 4 – Add User to NVR (Cloudvue Manager) searching for the MAC address. A search for the devices MAC address in Cloudvue Manager does not return any results. Product exacqVision Server Steps to Reproduce Perform all steps found in Knowledge Base… Continue reading Unable to Find MAC Address During Exacq Cloud Drive Archiving Setup
Exacq Cloud Drive 2.0 Setup
Cloud drive is a subscription plan available from an Exacq dealer for offsite, cloud based archiving of recorded video. Contact an authorized dealer to discussing pricing and plans. Minimum Client/Server Versions: Client: 22.03.1 Server: 22.03.0 The following instructions detail the steps to be performed in sequence. These steps are also detailed in our Video Library.… Continue reading Exacq Cloud Drive 2.0 Setup
Limitations of M-Series Servers
Overview: Known limitations of exacqVision M-Series servers. Issue: Cloud Drive is not supported.Starting in version 21.12, EdgeStor for Illustra Cameras connected to an M-Series server will no longer be supported. If the customer still wants to upgrade, please refer to:KB #1580 “How to update the M-Series recorder”KB #6655 “M-Series – Updating Exacq Software” Solution: There are NO available workarounds for these… Continue reading Limitations of M-Series Servers
2019-10-03 – exacqVision Cloud Drive
SCN-00000012 – Cloud Drive
SCN #SCN-00000012Title of SCNCloud DriveTRAC #Effective Version9.8Products AffectedServer, Client, MobileReason for Change (Summary)New Feature Change The Cloud Drive feature was officially added in 9.8, however we expect its use to grow with the release of the G-Series Micro. This document is intended to explain how the feature functions and what you’ll need to know to… Continue reading SCN-00000012 – Cloud Drive
ExacqVision Cloud Drive Data Sheet
Troubleshooting Cloud Drive
Note: Only H.264 streams are currently allowed for Cloud Drive. All other streams will be hidden on the Archiving Schedule page. Note: Audio is not currently supported for Cloud Drive. <br> As of 9.8, Cloud Drive technically runs as a side integration that is installed by default. This results in log files that are separate… Continue reading Troubleshooting Cloud Drive
Direct Archive Search Explained
exacqVision 7.8 introduced enhancements to video archiving to provide faster access to video and better manage bandwidth. Users closer to the archive location on the network can directly search video on the archive without routing data through the recorder. Direct archive search is available for any Exacq S-Series storage device and any third-party network share… Continue reading Direct Archive Search Explained