If a Q87-based Windows exacqVision unit experiences a BSOD with the reference Driver_Power_State_Failure, you should update the USB 3.0 drivers to at least 3.0.5.69. This will prevent the BSOD from occurring based on USB issues with the motherboard.
To install the driver, complete the following steps:
- Download the file from Intel.
- Right-click the .zip file and select Extract All.
- When the extraction is complete, open the containing folders and find Setup.exe.
- Right-click Setup.exe and select Run as Administrator.
- Follow the instructions to install the drivers.
- When the installation is complete, choose the option to reboot the server.
If you install the drivers and get a message from iusb3mon.exe during every startup, deselect the box next to Always Ask Before Running This File in the dialog box.
<br>
Q87-based-Windows-exacqVision-System-Driver_Power_State_Failure-BSOD.pdf