With Artificial Intelligence being used more often users may notice a spike in the analytic metadata being processed and stored. Here are our recommendations to manage this increase. Update exacqVision Server/Client Software Adjust Camera Settings Reduce DB retention period Disable Analytics Related Articles AESW-5987
Tag: Best Practices
Support Portal Articles – Best Practices
Template See: Support Portal Knowledge Base Articles – Creation Template <br> Guidelines Special Tags In addition to standard tagging the following specific tags control the exposure level of the post to various user groups on the support portal. <br> Standardized Spellings for Articles <br>
exacqVision Hardening Guide
Description A hardening guide is a supplemental document that is provided alongside installation instructions with a product. Product Solution A hardening guide is a supplemental document that is provided alongside installation instructions with a product. This hardening guide will outline the minimal necessary steps to ensure a secure installation of the product in a customer… Continue reading exacqVision Hardening Guide
Example Network Diagram for Multi-NIC Systems
Best practice for servers with more than one NIC includes isolating camera traffic to a separate scheme. This practice not only isolates camera bandwidth consumption from other network traffic, but also adds an additional layer of security to prevent workstation users from accessing cameras and video streams directly. Whether using separate network switches or creating… Continue reading Example Network Diagram for Multi-NIC Systems
Time Settings and Time Zone Information
Background Information The Windows or Linux (Ubuntu) operating system time of your exacqVision Server host should be set to the local time and time zone where it is located. It is often desirable to synchronize the system to a central time server, rather than rely on the internal clock of the recording server. There are… Continue reading Time Settings and Time Zone Information