In the ExacqVision Edge Server Trunk build version 21.06.114, We have improved our config persistence algorithm to guard against sudden power losses. you can download and use this version or wait until the next official release which is 21.09
Tag: Axis Cameras
Issues with Relays on Axis A8004-VE
After updating to 20.12 or 21.03 the relays don’t work for Axis A8004-VE Will be backpatched in 21.09, currently there is a DEV Build 21.06.107 https://trac.exacq.com/DVR/ticket/22891
How to Enable Edge Storage on Axis Cameras
The instructions below differ based on the firmware versions on your Axis cameras. Please check your camera’s firmware version prior to continuing. <br> Edge Storage recording is currently supported for recording based on motion events. Setting the camera(s) to continuous recording may produce unpredictable results. <br> Adding the camera to exacqVision: When adding your camera(s)… Continue reading How to Enable Edge Storage on Axis Cameras
Dewarping of Axis hemispheric cameras does not work through web service
Affected platforms exacqVision web service 7.4 <br> Symptom The Axis dewarping library uses OpenGL and therefor will not work when launched as a Windows service or without access to X Windows in Linux. <br> Workaround Run the webservice as an application rather than a service. In Windows:1. Start => Run cmd enter2. Run the command… Continue reading Dewarping of Axis hemispheric cameras does not work through web service