Archiving

Archiving allows you to create a copy of selected data on another storage device, whether it be an exacqVision S-series storage server, a user provided storage server, exacqVision Cloud Drive, an Amazon S3 account, or Wasabi S3 account. This video explains how to create a new archiving profile, establish the archiving task, then schedule the… Continue reading Archiving

Cloud drive relies on the bit rate, not the quality when archiving the cameras.

Description When choosing a subscription for a camera on a cloud drive, it relies on the bitrate, not the quality. Example: You are selecting a 4K subscription for an Illustra Flex2 4K Dome camera on the could drive.

Unable to Find MAC Address During Exacq Cloud Drive Archiving Setup

Description  After performing all steps found in Knowledge Base Article #7697 up to Step 4 – Add User to NVR (Cloudvue Manager) searching for the MAC address.  A search for the devices MAC address in Cloudvue Manager does not return any results. Product  exacqVision Server Steps to Reproduce  Perform all steps found in Knowledge Base… Continue reading Unable to Find MAC Address During Exacq Cloud Drive Archiving Setup

When trying to connect to S-Series archive target the status is “Disconnected”

Description When the Exacq NVR you are configuring to archive to an Exacq S-Series and the recording NVR is joined to a domain, there is a local Group Policy that must be configured to prevent receiving a ‘Disconnected’ status. Product Steps to Reproduce Expected Result Arching target is ‘Connected’ Actual Result Archiving target is ‘Disconnected’… Continue reading When trying to connect to S-Series archive target the status is “Disconnected”

Using gdisk to Fix Backup GPT Table Errors in Linux  

Description  When experiencing Errors partitioning additional storage after a RAID array has been expanded or partition issues with either Archiving or Extended storage drives on an S-Series Server.  Check the partitions for errors using parted.  Product  Steps to Reproduce  Expected Results  The results return the partition layout on all block devices with no Errors   Actual… Continue reading Using gdisk to Fix Backup GPT Table Errors in Linux  

Exacq Cloud Drive 2.0 Setup

Cloud drive is a subscription plan available from an Exacq dealer for offsite, cloud based archiving of recorded video. Contact an authorized dealer to discussing pricing and plans. Minimum Client/Server Versions: Client: 22.03.1 Server: 22.03.0 The following instructions detail the steps to be performed in sequence. These steps are also detailed in our Video Library.… Continue reading Exacq Cloud Drive 2.0 Setup

Unable to set archiving schedule

If all of the boxes for the camera are greyed out for a camera on the Schedule page under Archiving… Check to verify in the Exacq Client under Storage you DO NOT have a Expiration Configuration rule set; if you do remove it. Then go back to the Archiving Schedule page and select your cameras… Continue reading Unable to set archiving schedule

Archiving continually says “Disconnected” on Linux systems 12.04 and Older

When connecting an NVR running Ubuntu 12.04 or older to a newer S-series you may have issues with it connecting and displaying the “Disconnected” message on the archiving page; even thou everything is correct and systems running Ubuntu 14.04 or newer DO NOT have this issue. When you search the logs, you will see a… Continue reading Archiving continually says “Disconnected” on Linux systems 12.04 and Older