Enterprise Manager supports LDAP authentication with Azure Active Directory 

Azure Active Directory supports the LDAP interface when properly configured, and therefor LDAP can be used to sync the ExacqVision Enterprise Manager software with the Azure AD instance. Background Information: Lightweight Directory Access Protocol (LDAP) is an application protocol for working with various directory services. Directory services, such as Active Directory, store user and account… Continue reading Enterprise Manager supports LDAP authentication with Azure Active Directory 

AES Encryption Methods Supported For LDAP Connection

AES-128 and AES-256 encryption support for LDAP communication was added with the release of exacqVision Server 21.12.3. Versions older than that must use RC4 encryption. To determine if you are using the AES encryption or not. Check the logs from Exacq server for the StreamPi plugin, and if you are using the AES encryption and… Continue reading AES Encryption Methods Supported For LDAP Connection

Setting a primary group to an LDAP user

Issue If you have an LDAP group listed on the ExacqVision server, and you set this group as a primary group for a specific user. The Active Directory will not authorize this user to log in on ExacqVision software. Solution Remove this group from being the primary group of the user, or add this user… Continue reading Setting a primary group to an LDAP user