Input(***): Describe response failed (retcode 401) Description 401 is an HTTP error code for “Unauthorized”. For unknown reason this sometimes appears when the correct credentials are entered in the client. Notes Re-enter the password for the root account in the camera’s web interface.
Category: VivotekPI
Input(): Unrecognized resolution.
Input(): Unrecognized resolution. Description Server plugin does not like the resolution setting from the camera. Notes Enter camera web interface and change the resolution to match the IP Camera Integration test records.
Input #: Unsupported codec.
Input #: Unsupported codec. Description The camera is currently streaming in a codec that cannot be received. Notes Change the stream codec to one supported or factory default the camera.The IP8162 may set codec to “SVC” after a factory default. The camera doesn’t even support this stream. You must change the stream profile back to… Continue reading Input #: Unsupported codec.
Send|Receive failure – buffer overrun.
Send|Receive failure – buffer overrun. Description The available buffer space for communication was not able to send or receive the requested information. Notes Could be a resource limitation or anti-virus interference.