Description Reports stating the Axis dewarper sometimes shows up in our software and other times doesn’t for different models. 2nd issue stated that the generic dewarper is “elongated” or distorted when zooming in via digital PTZ and panning or tilting the camera. Product Steps to Reproduce tried different formats H.264/H.265tried different resolutions–>no changetried Ceiling/WallTried Digital… Continue reading Added Axis Dewarping on Axis M Series Cameras
Category: AxisPI
update config query delta attribute error
update config query delta attribute error Description This message can usually be ignored.%BR% The Axis plugin is trying to process XML configuration coming to it, but the XML is missing a ‘delta’ attribute. If the XML doesn’t have the ‘delta’ attribute, the plugin ignores the XML message and moves on.%BR% This may occur from devices… Continue reading update config query delta attribute error
%1 will be using VMD4 for Motion Events
%1 will be using VMD4 for Motion Events Description %1 = IP Address of camera. Indicates that VMD4 is being used for motion event detection. Notes This is a normal message.
%1 send error 110
%1 send error 110 Description %1 = IP address of camera.110 is a Linux C Error code “ETIMEDOUT 110 /* Connection timed out */” Notes This occurs on the send side of the data rather than the receive side, which is why it is a send error.
H.264|MPEG-4 GOV length is %
H.264|MPEG-4 GOV length is % Description GOV (Group of Video) is the I-frame interval for the video stream. Notes This is a normal message.
Request was denied by the device. Make sure the correct credentials have been entered
Request was denied by the device. Make sure the correct credentials have been entered Description With Axis firmware 5.70 and later with encryption mode enabled, an Axis device could take up to five minutes (the default setting for IP reconnection in exacqVision) to start streaming. Notes Workaround: Wait for the IP reconnection period to elapse… Continue reading Request was denied by the device. Make sure the correct credentials have been entered
*XXX buffer full state = 0 content true
*XXX buffer full state = 0 content true Description Unable to buffer larger than 2MB image size. Older version of Server (pre 8.2) had a smaller buffer for video frames. Notes Update beyond 8.2, or reduce either the quality or record resolution.
%1 unexpected marker 0x01 at offset %2 in SEI data
%1 unexpected marker 0x01 at offset %2 in SEI data Description This means that the data in the stream header is inconsistent. Probably due to network traffic problems and packet loss. The user data can include time stamp and motion information%BR%%BR% %1 – camera name%BR% %2 – offset number%BR%