ExacqVision Audit Logs Filling Linux OS Drive Due to Excessive LDAP or RTSP Login Failures

Summary On Linux‑based ExacqVision servers, the operating system drive may fill up because Exacq’s internal audit logs grow uncontrollably. The most common cause is repeated authentication failures generated by: Symptoms Administrators may observe: Root Cause ExacqVision logs every authentication event. When LDAP or RTSP authentication repeatedly fails, the audit log grows rapidly.Common LDAP-related causes Resolution… Continue reading ExacqVision Audit Logs Filling Linux OS Drive Due to Excessive LDAP or RTSP Login Failures

Acti A426 motion not working on Exacq 24.12.7.0

Introduction ACTI A426 camera on Server version 24.12.7.0 had motion recording issues, where they would not record while the camera gui would register motion events.Updating the motion mask from the client reverted after saving. Tested Version Server Version: “25.1.6.0”TESTED roll back to 24.06 – motion was still not working. Platform LINUX UBUNTU 18.04.1 LTS Steps… Continue reading Acti A426 motion not working on Exacq 24.12.7.0

Samsung PNM-C32083RVQ Issue with Exacq Server

Description  Currently the Samsung PNM-C32083RVQ is seeing some issues with connecting and causing client to drop the connection to the server. Product  Solution We are aware and have fixed this issue with later build.ExacqVisionServer_25.1.1039.0_x64 was tested and successfully resolved the issue. We are currently waiting on a RC build we can share with customers or… Continue reading Samsung PNM-C32083RVQ Issue with Exacq Server

FLIR Camera Motion Stops Recording Motion Events

Description  Motion will stop working on FLIR models after updating from exacq Server 24.09.5.0 to exacqServer 24.12.7.0. Product  CAMERAS:Flir FC-317-IDFC-324-IDFC-332-ID Steps to Reproduce  Update exacqServer to 24.12.7.0 motion events will stop working properly. Expected Results  Motion should work. Actual Results  Motion Stops working upon updates to 24.12.7.0. Solution Test build exacqVisionServer_24.12.2239205.0_x64 is working25H1 will house… Continue reading FLIR Camera Motion Stops Recording Motion Events

Avigilon Camera Motion Detection Fails on exacqVision Server 24.12.7.0

Description  When updating Exacq Server to 24.12.7.0 motion events will stop registering in the Camera Setting page under status last motion event. Motion Events are not being recorded. Product  Steps to Reproduce  Expected Results  Actual Results  Solution

Added Axis Dewarping on Axis M Series Cameras

Description  Reports stating the Axis dewarper sometimes shows up in our software and other times doesn’t for different models. 2nd issue stated that the generic dewarper is “elongated” or distorted when zooming in via digital PTZ and panning or tilting the camera. Product  Steps to Reproduce  tried different formats H.264/H.265tried different resolutions–>no changetried Ceiling/WallTried Digital… Continue reading Added Axis Dewarping on Axis M Series Cameras

Hanwha PNM-C32083RVQ Connection to Server and Motion Stops Working

Description  Hanwha will not allow motion to work properly with Exacq Server 24.09.4.0 as long as the camera is on fw 23.01.04-20240417-R929 due to a NTP issue found. Another issue reported is the connection status will throw errors to indicate it is not connected properly.NOTE:FW 23.01.01 obtained from Hanwha (which will be the official release… Continue reading Hanwha PNM-C32083RVQ Connection to Server and Motion Stops Working

Samsung PNM-C34404RQPZ Connection Issues

Description There have been several reports of connection issues with the Samsung PNM-C34404RQPZ. Reports of the units rebooting upon connecting it to the client and which plugin to utilize. Product  Exacq Server 24.03.7.0Camera Info: Samsung PNM-C34404RQPZFW used: 23.01.04_20240417_R650 https://www.exacq.com/integration/ipcams/#getCameraRecord=901b747e-fcbf-5464-7543-5aeb7ae3afe8~nstep_id=step-3 Steps to Reproduce  In the Client go to Add IP Cameras under the configuration. Add the first… Continue reading Samsung PNM-C34404RQPZ Connection Issues

H265 Motion Detection Fails on Panasonic WV-S8531N

Description  The Panasonic WV-S8531N fails to detect motion when using H265 option. Product  ExacqVision Server Steps to Reproduce  Expected Results  Motion is detected and video records. Actual Results  Motion is not detected and video is not recorded. Solution Updating firmware to S8531_202ES allowed the camera use Motion with H265 format on Server 22.09. AES-146 <br>

Arecont Camera 12176DN on firmware 65216 is Causing the Video Stream to Timeout

Description  Arecont Camera 12176DN on fw 65200 is causing the video stream to time out and the stream is reconnecting. CGI access to the camera is fine. Product  Steps to Reproduce  Connect to the camera and let it record. The video stream is timing out and the stream is reconnecting. CGI access to the camera… Continue reading Arecont Camera 12176DN on firmware 65216 is Causing the Video Stream to Timeout