Category: Highlighted
exacqVision 25.1P1 Release Bulletin
exacqVision 25H1 Release Bulletin
exacqVision Mobile – Getting Started & Server Connections
This video shows users how to connect to exacqVision Servers and manage Server connections.<br><br> Chapters:<br>00:00 Intro<br>00:25 Connecting to your first server<br>00:39 Connecting with an access code<br>01:12 Connecting using a URL<br>01:34 Quick View<br>02:05 Connecting to additional servers<br>02:22 Managing server connections<br> <br>
The Importance of UPS Systems
What is a UPS? Uninterruptible Power Supplies (UPS) provide battery powered backups to critical systems in the event of a loss to the building’s power. Why using UPS is critical The points listed above affect not just exacqVision systems, but can affect any computer system or modern electronic device. Consider placing all mission critical systems… Continue reading The Importance of UPS Systems
Deprecation of Legacy Installers – exacqVision 24.03 Update
As part of the exacqVision 24.03 software release, we are announcing the deprecation of specific installers that were previously part of the collection of software downloads available on the Exacq web site, https://exacq.com. What installers are being retired? On both Windows and Ubuntu – the 32-bit installers, also known as “x86” installers, of server, client,… Continue reading Deprecation of Legacy Installers – exacqVision 24.03 Update
Where can I access Training Courses?
Checking Your Case Status
Did you know that you can check the status of cases you created within the Exacq Support Portal? After logging into the Exacq Support Portal, open the Support menu. Select My Cases from the menu. A list of cases that appears will list the status of the case as open or closed. Further details can… Continue reading Checking Your Case Status
Using SSL with exacqVision Web Service (Linux)
Version 8.4 and Higher Follow the instructions in Article 1002 to configure HTTPS support in the Web Service. <br> Version 8.2 and Lower SSL, a security system combining authentication and encryption, is used to protect communication between a web server and client. Enabling SSL on a web server allow all clients connecting to that server two key… Continue reading Using SSL with exacqVision Web Service (Linux)
How do I apply a license to an exacqVision Server?
Only one license key may be applied on each system at a time. This license key includes information on the number of licensed IP Cameras the system is permitted to use as well as the specific system it is assigned to. For information on increasing your licensed number of cameras or changing your license level,… Continue reading How do I apply a license to an exacqVision Server?