Categories
Video Library Knowledge Support Demo Support exacqVision Enterprise exacqVision Client exacqVision Server exacqVision Mobile exacqVision Webservice Categories exacqVision Hardware Products exacqVision Integrations

2022-03 March Quarterly Release Training

exacqVision Client 

* Enhancement – Show toast for all web panels that fail cert setting checks. 

* Enhancement – Added separate archive rate and upload rate fields for archive targets that report them. 

* Enhancement – Add Enter to the default DCZ joystick profile 

* Enhancement – Added Select Camera joystick button action 

* Enhancement – Added numeric key joystick button actions 

* Enhancement – Support up to 128 joystick buttons on Windows 

* Enhancement – Added new indicator to suggest enabling password strengthening and augmented authentication. 

* Enhancement – Add camera web configuration page within the client. 

* Enhancement – Updated status text for cloud drive 2.0 configuration process 

* Enhancement – Added indicator for new cloud drive camera subscriptions available  

* Enhancement – Added indicator for incomplete archive configuration 

* Enhancement – cloud drive help hyperlink on Archives page navigates to user manual  

exacqVision Server 

* Enhancement – itv2pi – Add support for DSC PowerSeries Pro 

* Enhancement – SysmgmtPI – Include raw output from sysinfo script in server log at LOG_DEBUG level, to include in support exports. 

* Enhancement – brivopi – Support Brivo access control system 

* Bug Fix – SoundPI – Fix crash on opening input stream in Linux. 

* Bug Fix – SoundPI – Fix config shifting in both Windows and Linux that broke recording and event linkages with record audio target. 

* Bug Fix – SoundPI – Eliminate low-level PortAudio, PulseAudio, and libasound warnings. 

* Bug Fix – SoundPI – Improve inconsistent number of detected devices, and ambiguous naming. 

* Enhancement – onvifnvcpi – Add Motion topics for X2 Redvision cameras. 

* Enhancement – onvifnvcpi – Add support for Turing-U motion and analytics. 

 * Enhancement – onvifnvcpi – Add support for SCW uniview alias 

* Enhancement – ActiPI, AxisPI, SamsungPI, illustra3PI, onvifnvcpi, panasonicpi, SonyPI, VivotekPI, ccurePI, kantechpi – Encrypt passwords stored in config. 

 * Enhancement – archivepi – Updated to Smartvue SDK 22.1.0 and latest bundle.crt 

* Enhancement – illustra3pi – Add support for the queue analytic 

* Enhancement – hikvisionpi – Support displaying and modifying motion mask when camera is in corridor mode. 

* Enhancement – illustra3pi – Support Tamper detection. 

* Enhancement – samsungpi – Add override for using the camera timezone 

 * Enhancement – itv2pi – Add the option to filter out null zones since they can cause confusion for users. 

* Enhancement – archivepi – Cloud drive related certificate is no longer removed during restart 

 * Enhancement – axispi – Support radar detection events

* Enhancement – psfpi – Throttle audio as well as video when the system is throttling. 

* Bug Fix – psfpi – Changed to time based cache rather than packets to address an issue related to push to talk 

exacqVision Web Service 

* Bug Fix – Corrected version of mobile interface that is packaged. 

exacqVision Mobile 

* Enhancement – For Search Only, display No Video Available instead of Unknown Error 

* Enhancement – Live scroll view. 

* Enhancement – Reorganize configuration pages 

* Enhancement – Display messages below icons on video error 

* Enhancement – Added support for searching cloud drive 2.0 

* Bug Fix – Search Timeline metadata should be displayed by default

* Bug Fix – Attempt to reconnect to web servers when internet connection comes back 

* Bug Fix – Stop resubscribe to video on layout change 

* Bug Fix – Added space for the iOS home bar 

exacqVision Enterprise Manager 

* Enhancement – Add Reset importer failure counter after some time 

* Enhancement – Update JQuery to 3.6.0