IP Camera Detection Fails If Using Multiple Addresses on Same Interface

Symptom:

IP camera detection fails.

<br>

Problem:

If more than one IP address has been assigned to the same network interface on a Windows system exacqVision Server may fail to use correct IP address, thus camera detection fails. Linux is not known to be affected.

<br>

Solution:

Option 1: Temporarily remove all but one IP address from the interface. Restart the server service and re-attempt discovery. 

Option 2: Update exacqVision Server to version 9.4 or later. 

<br>

IP-Camera-Detection-Fails-If-Using-Multiple-Addresses-on-Same-Interface.pdf