when trying to connect to the S3 internal solution via the Exacq archiving page instead of the standard AWS S3 bucket the system couldn’t establish the connection to it.
The standalone S3 solutions are not supported via Exacq Software and the only S3 solution that supported till server version 21.03 is the AWS S3 and we are working on adding this feature in the future builds
Recently tested:
Wasabi S3
Connection would fail with errors:
TM=12:43:19.359;LV=25;PI=390000;TX=[https://security-8.s3.us-central-1.wasabisys.com] begin connect attempt.
TM=12:43:19.359;LV=25;PI=390000;TX=[https://security-8.s3.us-central-1.wasabisys.com] end connect attempt.
TM=12:43:19.434;LV=25;PI=60000;TX=LDAP query: (servicePrincipalName=HOST/exacq-nvr-test.edu)
TM=12:43:19.462;LV=75;PI=390000;TX=Invalid S3 path = https://security-8.s3.us-central-1.wasabisys.com
TM=12:43:19.462;LV=50;PI=390000;TX=[https://security-8.s3.us-central-1.wasabisys.com] Target interface could not be created.
Tickets:
19422
22794
AES-45