Certain LDAP Condition Causes exacqVision Crash

In exacqVision 5.4 and earlier, the following configuration can cause an exacqVision system to crash:

*On the Add Systems page, the Use Single Sign-On option is selected for the server.

*The LDAP tree that the system uses for authentication contains other LDAP servers that serve sub-trees.

*One or more the sub-tree LDAP servers aren’t running or aren’t allowing connections, which makes those parts of the LDAP tree unsearchable.


If a crash report is enabled and available, you will see that the “core” crashed in nsldap32v60.(dll/so).


NOTE: Starting with exacqVision 5.6, this configuration should not cause a system crash.

<br>

Certain-LDAP-Condition-Causes-exacqVision-Crash.pdf