2024-09 September Quarterly Release Training

<br>

exacqVision Server

  • Bug Fix – Fixed insertion of objects lacking metadata or bounding box
    (AESW-9440)
  • Bug Fix – Improvements to event size estimates for bookmarks
    (AESW-11010)
  • Bug Fix – illustra3 and illustramultipi fixed issue where Alarm 2 status would not change after being canceled
    (AESW-10146)
  • Bug Fix – illustra3 and illustramultipi fixed issue causing edgestor backfill to hang
    (AESW-9581)
  • Bug Fix – Onvif, fixed issue preventing simultaneous PTZ
  • Big Fix – Onvif, fixed excessive pullpoint logs on errors
    (AESW-10727)
  • Bug Fix – Onivf, fixed potential PTZ disconnects
    (AESW-11469)
  • Bug Fix – psfpi, fixed potential hang when evAPI attempts to cancel search
    (AESW-10961)
  • Bug Fix – Samsungpi, fixed crash on disabled device during connection
  • Bug Fix – Samsungpi, fixed potential crash when connecting to newer devices
  • Enhancement – Support Area Zoom on Axis M5000-G PTZ camera
    (AESW-10568)
  • Enhancement – eventpi, new event indicates thinning occurred, includes event linking sources
    (AESW-7651)
  • Enhancement – Installer adds firewall rules added for failover and failback
  • Enhancement – Improved analytic parsing
  • Enhancement – Provide the analytic type to core
  • Enhancement – Improved handling of transport errors
    (AESW-10120)
  • Enhancement – New SOAP calls for Onvif Profile M and S conformance
  • Enhancement – remotepi, move connection to production switchboard service
    (AESW-9771)
  • Enhancement – Additional logging around LDAP reauth queries
    (AESW-9769)
  • Enhancement – Improved performance by reducing amount of analytics sent from server to client
    (AESW-7715)
  • Feature – Support for Wasabi S3 as archiving target
    (AESW-5814, AESW-10924)
  • Feature – Support added for Axis Thermometry
    (AESW-8816, AESW-8918)
  • Feature – Illustra LPR Support
    (AESW-6504)

exacqVision Client

  • Bug Fix – Manage the preferred MAC address in License panel
    (AESW-11267)
  • Bug Fix – Fixed issue where exacqReply controls did not appear until window was resized
    (AESW-9992)
  • Bug Fix – Clear grid dropdown, to fix issue where drop-down menus duplicate entries
    (AESW-10923)
  • Bug Fix – Fixed issue with Oldest Desired Content of Cloud Drive
    (AESW-8097)
  • Bug Fix – Fixed issue of event forward button being disabled when skipping ahead
    (AESW-8958)
  • Bug Fix – Fixed issue of client crash when selecting Find Camera when creating a new View
    (AESW-10038)
  • Bug Fix – Fixed client crash when selecting audio in Add Video panel
  • Bug Fix – Fixed issue of auto play not working in Timeline search
    (AESW-8529)
  • Enhancement – Remote Connections, found on navigation tree
  • Enhancement – Added Mobile Optimized Streaming panel for Remote Connections
  • Enhancement – New toast message indicating event thinning has occurred
    (AESW-9871)
  • Enhancement – Client improvements to amount of analytic data passed between server/client
    (AESW-7716)
  • Enhancement – Support “horizontal flip” for Storage page to accommodate storage layout for new Avnet systems
    (AESW-10562)
  • Enhancement – Apply our security standards to Bodyworn password fields
    (AESW-1575)
  • Feature – Support for Wasabi S3 as archiving target
    (AESW-11025)

exacqVision Web Service

  • Bug Fix – Fixed 24.03 issue where iPAD experienced video buffering and timeout errors
    (AESW-10945, AES-839, AES-863, AES-909)
  • Bug Fix – Web client supports session timeout detection, respects the login token
    (AESW-9753, AES-774)

exacqVision Enterprise Manager

  • Bug Fix – Add missing pagination endpoints
  • (AESW-11414)

Exacq Mobile 3

  • Bug Fix – Fixed issue with video failing to play after one hour
  • Enhancement – Added notification to point users to new exacqVision Mobile app
    (AESW-9166)

exacqVision Mobile

  • exacqVision Mobile requires Server version 24.09 or higher
  • Remote Connectivity requires Client 24.09 or higher as the Client is needed to connect to the cloud switchboard and generate access codes
  • If SSA expiration or OS requirements prevent updating to Server 24.03, users will need to continue using Exacq Mobile 3, with the exacqVision Web Service

Exacq Hardware

Hardware Revisions

  • C-Series 16S & 32S
  • G-Series Micro
  • G-Series PoE 8ch & 16ch
  • Q-Series Desktop & Desktop Hybrid
  • A-Series 2A & 2A Hybrid  (no RAID)
  • A-Series FA & FAR  (RAID)
  • X-Series 1U & 2U  (RAID)

exacqVision Advantage

  • Provides free exacqVision licensing on BBE hardware for most models of Illustra Flex and Pro cameras (Gen3, Gen4, and future generations).
  • Does not apply to the Flex Gen3 Multisensor, which is ONVIF only, does not have the Illustra API

Illustra

  • New Pro camera models providing LPR on the edge
    • Bullet IPS05-B12-LPR4
    • Dome IPS05-D12-LPR4

<br>