Categories
Video Library Knowledge Support Demo Release Notes Support exacqVision Enterprise Other exacqVision Client exacqVision Server Categories exacqVision Webservice Products exacqVision Integrations

2023-03 March Quarterly Release Training

ExacqVision Server

Bug Fix – Fixed PTZ preset administration for custom users to create presets for analog cameras (AESW-4357)

Bug Fix – Fixed monitoring RAID background tasks, like consistency checks and background initialization (AESW-4387)

Bug Fix – Fixed reporting incorrect RAM, was displaying MB instead of GB (AESW-2498)

Bug Fix – actipi – Reduce metadata channel reconnects for cameras with S3L chips, this caused cameras to stop recording after a while (AESW-4327)

Bug Fix – illustramultipi – Fixed ability to enable motion zones per sensor, accommodated changed to camera firmware (AESW-4456)

Bug Fix – illustramultipi – Fixed direct input/output triggers, fixed output numbering that was preventing trigger status from updating (AESW-3474)

Bug Fix – onvifnvcpi – Fixed motion issues with AVCostar-Contera (AESW-4464)

Bug Fix – onvifnvcpi – Increased maximum SOAP read size to accommodate Clinton encoders, see Enhancements (AESW-3474)

Enhancement – Modified all emissions from eventpi and notifypi to use separated IDs rather than compressed IDs, fixed in part, this is an enhancement to affect problems with searching the event database with very large amounts of records (AESW-3333)

Enhancement – Added camera detection of several Illustra Standard cameras to be discovered as Illustra3
(AESW-1668)

Enhancement – axispi – Added support for color metadata (AESW-1725)
Only vehicle color is currently provided by Axis

Enhancement – illustra3, illustramultipi – Added support for “final color” (AESW-2850, AESW-2844)

Enhancement – samsungpi – Added support for Area Zoom (AESW-4003)

Enhancement – onvifnvcpi – Added support for Advidia cameras (AESW-3521)

Enhancement – onvifnvcpi – Added support for Clinton Electronics encoder (AESW-2489)

ExacqVision Client

Bug Fix – Don’t reorder keywords when building conditions panel tree
Ensures ‘Upper Clothing Color’ is listed above ‘Lower Clothing Color’ in Filters (AESW-4502)

Bug Fix – Allow live analytic keyword colors to be processed before bounding boxes (AESW-4458)

Bug Fix – Fixed an issue with display of multiple trigger events (AESW-3861)

Bug Fix – Fixed issue saving image from Live view where OSD background color was removed from the saved image (AESW-4277)

Enhancement – Support for “final color”, choose search type based on “final color” (AESW-3345)

ExacqVision Web Service

Bug Fix – Updated nvrg version to fix group type retrieval (AESW-3340)

Bug Fix – Updated nvrg version to fix a soft trigger bottleneck (AESW-3816)

Enhancement – Disabled search playback in browser client until buffer threshold is reached (AESW-3622)

Enhancement – Enabled ability to detect an invalid session in browser client (AESW-3621)

ExacqVision Enterprise Manager

Bug Fix – Removed architecture change logic from NSIS (AESW-491)

Bug Fix – Support added for Windows authentication login for MS-SQL (AESW-3378)

Illustra

Enhancement – New Pro Gen4 6.0 firmware adds new Object Classes
Trolley, Backpack, Handbag, Suitcase

Enhancement – Improved face detection

Enhancement – “Final color” sent after object tracked leaves FOV