2022-09 September Quarterly Release Training

*There appears to have been a slight bug in the presentation recording where the video recording did not capture the videos being played on the screen. The links below will provide access to the PowerPoint file and individual demonstration videos.


ExacqVision Server

Bug Fix – Removed limit of 256 devices displayed for Access Control plugins, only visible when using Access Control with Associations or Maps

Bug Fix – Fixed issue with Illustra3 and Illustramultipi that could cause cameras to be stuck in a Connecting state after reboot

Bug Fix – Fixed issue where Edgestor was not backfilling data from Illustra3pi cameras due to Edgestor crash, leaving gaps on server recordings

Bug Fix – Fixed quality setting for Illustramultipi

Bug Fix – Fixed issue with trigger inputs/alarm outputs for Illustramultipi

Bug Fix – Added retry logic on API errors for napcopi, Napco uses IIS which has a recycle time that caused authentication to fail, fix adds retry logic if error received

Bug Fix – Fixed issue causing credentials for RTSP Server not to be updated properly

Bug Fix – Corrected issue where Date/Time page was greyed out on Win7 machines

Bug Fix – Fixed issue where Dynacolor devices may repeatedly reset after user presses Reset button on PoE port in Client.

Bug Fix – Fixed viewing Live Analytics for Flex3 cameras

Bug Fix – Fixed issue where closing video stream did not close metadata stream from Illustra3pi

Bug Fix – Fixed propagating motion alarms on disabled context streams on Illustra3pi

Bug Fix – Fixed setting transport and re-reading URL for continuous metadata from Illustra3pi

Bug Fix – For Illustra3pi and Illustramultipi, use friendly name for analytics that provide bounding box

Enhancement – Added motion support for March Network cameras using Onvif

Enhancement – Support for Redvision RVX2 added to Onvif plugin

Enhancement – Support for Sunell with transport RTSP added for Onvif

Enhancement – Improvements made for Last Motion event on context streams

Enhancement – Adjustments made to parsing Audio Output name for Illustramultipi

Enhancement – Removed eDVR and XDVAPI license handling

Enhancement – §Homogenized analytic values for Axis, Samsung/Hanwha, Tycodlpi; Presents “Person” instead of “Human”, “Bicycle” instead of “Bike”

Enhancement – Added support for Axis’ new metadata style used in their 11.0 firmware

Feature – Added support for vehicle and clothing color provided by Illustra3pi and Illustramultipi cameras

ExacqVision Client

Bug Fix – Reset search item flags when sending new search requests, fixes issue when Search stops working if server connection lost mid-search

Bug Fix – Don’t send scrub request if waiting for summary response

Bug Fix – Prevent potential crash on Association config page if a camera with associations was deleted

Bug Fix – Initialize Digital PTZ settings to Client settings when plugin does not send them, related to changes made for body worn cameras

Bug Fix – Prevent toast messages for streaming BWCs on system disconnect

Bug Fix – Reset camera connection status on system disconnect

Bug Fix – Disabled BWC audio devices on Audio configuration page

Bug Fix – Prevent security integration sources from being displayed twice in bookmark editing tree

Bug Fix – Fixed potential crash when adding new IP serial port and config update occurs

Bug Fix – Prevent client crash with double-clicking on grid divider in List View

Bug Fix – Prevent client crash on OSX when clicking calendar controls

Bug Fix – Fixed issue with export failure if config page options in settings file

Enhancement – Prevent some analytic search filters that didn’t make sense, non-sensical combinations of operator logic

Enhancement – Don’t request event data in response to Show Conditions panel, caused Search to stop working when connection to Server was lost mid-search

Enhancement – Display analytic colors above bounding boxes

ExacqVision Web Service

Bug Fix – Added libreadline8 dependency for the Ubuntu 22.04 installer

Bug Fix – Fix made to data races related to search and discovery

Bug Fix – Update search session keep alive when search frame is retrieved

Enhancement – Add search only status to cameras and audio streams

ExacqVision Mobile

Bug Fix – Fixed issue where Number of Servers Connected displayed in menu bar was incorrect

Bug Fix – Disable Autocorrect for Add Server page

Bug Fix – Removed Delete icon from Focus View mode

Bug Fix – Accidental scrub bar touches open Focus View

Bug Fix – Fixed issue with truncated camera pagination

Bug Fix – Fixed issue where rotating to landscape display and back made bottom row OSDs disappear

Bug Fix – Fixed issue where software was crashing when searching using server time

Bug Fix – Corrected issue where Views on iOS were not loading video

Bug Fix – Case sensitive issue on Add Server page, client did not handle adding system with capital letters in address

Bug Fix – Mobile app Login button not responding to EM sync login

Enhancement – Hide Search Only cameras from Live

Feature – Remove the data usage prompts and data collection, temp removal for launch due to requirements by Apple

ExacqVision Enterprise Manager

Bug Fix – Fixed showing deleted servers in the search results

Bug Fix – Fixed server configs from being checked for failover or updates