The Event monitoring trigger is not switching the video

The Event monitoring trigger is not switching the video

Description

The Event monitoring trigger is not switching the video the first time if you run it while another trigger works.

Reproducing the issue:-

  • creating Two event monitoring profiles using the Video Panel/View type and setting two soft triggers to trigger it manually, then set the action type to “switch the video”
  • Going to the live view and running the event monitoring, run the first soft trigger, then try to run the second one. It will not work the first time, and you have to disable the second trigger, then re-enable it again, which will make it works, and switch to the second view.

Resolution

This issue has been fixed in version 23.03