Description
After performing all steps found in Knowledge Base Article #7697 up to Step 4 – Add User to NVR (Cloudvue Manager) searching for the MAC address. A search for the devices MAC address in Cloudvue Manager does not return any results.
Product
- exacqVision Server
Steps to Reproduce
- Perform all steps found in Knowledge Base Article #7697 up to Step 4 – Add User to NVR (Cloudvue Manager) searching for the MAC address.
- Access Cloudvue Manager
- Select Search then Search Video Devices
- Enter the MAC address of the NVR and press enter to search
Expected Results
- MAC address is found
Actual Results
- MAC address is not found
Solution
- In the exacqVision Client delete the archive target
- Change the following line in archivepi.xml to ensure the system is using the endpoints used to reach Cloud Drive 2.0
Default Paths
Linux
/usr/local/exacq/server/archivepi.xml
Windows
C:\Program Files\exacqVision\Server\archivepi.xml
Change the following line in archivepi.xml
From
Defaults Type="4" Address="https://exacq-messaging.cloudvue.com" SearchAddress="https://exacq-gateway.cloudvue.com/v1/exacq"

To
Defaults Type="4" Address="messaging.cloudvue.com" SearchAddress="gateway.cloudvue.com"

- Re-create the archive target using the instructions from Knowledge Base Article #7697