Issue
If Exacq Enterprise Manager services on Windows are not starting and giving this message

Usually, it’s going to be a user privileges issue, and the user that is used for running the service is not able to start it
Solution
Sometimes in the domain environment, the service users will be restricted and will not have the permission to run the services and will need to change the login user to an admin user from the login tab for each service in order to make it works

This solution should work also for
ExacqVision Server
ExacqVision Webservice