AES-128 and AES-256 encryption support for LDAP communication was added with the release of exacqVision Server 21.12.3. Versions older than that must use RC4 encryption.
To determine if you are using the AES encryption or not.
Check the logs from Exacq server for the StreamPi plugin, and if you are using the AES encryption and the Server is not able to decode it then it would show you these logs
StreamPI Warning Encryption type: aes-cts-256-sha1-96 (occurs 58811 times)
StreamPI Warning Unable to decode encrypted ticket (occurs 33140 times)
StreamPI Warning Unable to decode encrypted element (occurs 22007 times)
Another method to check
From the Active directory in the DC, go to the binding user and right-click on it then properties, then navigate to the Account tab

If you are using the AES encryption, then you should have the AES 128 or AES 256 or both checked