Unexpected Throttling, Low Memory and Server Reboot

Description

In exacqVision Server versions 21.09 and 21.12 if audio outputs or push to talk are used it can cause a slow memory leak every minute. This will eventually cause the server to throttle and eventually hang or reboot.

Product

  • exacqVision Server 21.09
  • exacqVision Server 21.12

Solution

Upgrade exacqVision Server to RC 21.12.3 or higher, which contains enhancements which should resolve the issue. 


12/08/2021
v21.12.1

  • Enhancement – psfpi – Throttle audio as well as video when the system is throttling.

01/14/2022
v21.12.3

  • Bug Fix – psfpi – Changed to time based cache rather than packets to address an issue related to push to talk

<br>