M-Series – Updating exacqVision Software

In order to comply with the NDAA  “National Defense Authorization Act”, a two-step process is required to update an M-Series. First you must upgrade to version 20.03, then the server and webserver can be upgrade to the latest version. exacqVision Client versions higher than 20.03 are not supported.

  1. Install or upgrade exacqVision Server, exacqVision Client and exacqVision Web Server to version 20.03
  2. Upgrade exacqVision Server and exacqVision Web Server to version 21.09.

Note: The exacqVision Client version should not be updated past version 20.03

Upgrade Paths

Local Client – 20.03 only
Server – 20.03 > 21.09 or above
Web service – 20.03 > 21.09 or above

Additional Resources

Knowledge Base Article #1580 “How to update the M-Series recorder”