Factory resetting the bios for G-Series Micro

IMPORTANT: This article reflects G-Series Micros built prior to mid-2024.

To factory reset the bios for G-Series Micro, you need to follow these steps:-

1-Unplug power cable from the Unit

2-Remove the 4x Phillips Chassis screws

3-Remove bottom and top cover

4-Remove the RAM stick

5-Plug in power cable (should turn on automatically), and Wait ~10 seconds

6-Unplug power cable

7-Assemble back the RAM stick

8-Carefully unplug the RTC Battery from the 2pin connector

9-Plug power cable (should turn on automatically)

10-Shutdown the PC

11-Unplug the power cable

12-Plug the RTC Battery back in

13-Plug Power cable

BIOS settings should be reset to defaults now