Skip to content

Exacq

Support Portal CMS

The camera is showing connected but not streaming videos

If the camera is connected to ExacqVision Server and showing connected on the add IP camera page but not streaming videos and showing acquiring video. That means the RTSP streaming port may need to be opened on the Firewall, normally 554

Published May 17, 2021By Mena Awed
Categorized as Knowledge Support, Support, exacqVision Server, Categories, Products Tagged RTSP Stream, Port, Level2, 5602, Firewall, IP Cameras

Post navigation

Previous post

RtspServerPI may not be installed on Linux

Next post

Certain Illustra models may cause recording to stop

Recent Posts

  • Windows 7 Remote Connections
  • Associations Not Allowed to be saved as Momentary or Sustained Option
  • AVCostar (Arecont) AV20576RS camera model fails to decode H265 in ExacqVision
  • Illustra Edge Analytics
  • Hanwha Edge Analytics
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
  • Remote Connection