ONVIF PTZ camera with two streams may display as two different cameras even if “Manage all streams as quality” is checked

Product

exacqVision Server 6.2 to 7.2.3

<br>

Symptom

ONVIF PTZ camera with two streams may display as two different cameras even if “Manage all streams as quality” is checked. This is because the XML is reporting the secondary context as being an independent PTZ which is something generally used for fisheyes where PTZing one stream doesn’t PTZ the other streams.

<br>

Workaround

No workaround

<br>

Resolution

Update exacqVision Server to 7.4.0

<br>