exacqVision Server fails to start

Affected platforms

exacqVision Server 9.8

<br>

Description

When a file “C:\Program” exists, the Windows Service Control Manager (SCM) will fail to start the exacqVisionServer service.

<br>

Workaround

Perform the following steps:

  1. Delete the file “C:\Program”
  2. Rename C:\Program Files\exacqVision\Server\scripts\sysinfo.ps1 to sysinfo.ps1.bak
  3. Start exacqVision Server service

<br>

Resolution

Update to exacqVision Server 19.03.0 or higher