ACTi Encoder Multistream Connectivity

ACTi encoder connections require port numbers along with IP addresses to connect to multiple streams (where available).The port numbers for each stream on the encoder should increase incrementally starting with 800.

For example, if the IP address of an encoder with four analog streams is 192.168.101.25, the following IP and port number combinations must be entered on the exacqVision Client camera configuration page to connect the stream to the client:

  1. 192.168.101.25 port #800
  2. 192.168.101.25 port #801
  3. 192.168.101.25  port #802
  4. 192.168.101.25  port #803

<br>

ACTi-Encoder-Multistream-Connectivity.pdf