Settings for motion detection sensitity on Samsung cameras may appear different when deleting and re-adding camera

Description

exacqVision displays a value 1-100 for motion sensitivity. The camera itself only uses a 1-10 scale. When the user sets the sensitivity to 23, the actual value maps to 2, but the GUI still displays 23. If the camera is deleted and re-added, the sensitivity would display 20, rather than 23.

<br>

Settings-for-motion-detection-sensitity-on-Samsung-cameras-may-appear-different-when-deleting-and-re-adding-camera.pdf