VADP Upload Fail on Vivotek Cameras

After formatting an SD card for a Vivotek camera, the VADP upload can fail with the following error:

Create “/mnt/auto/CF/vadp” failed
Upload module failed
Upload VADP package failed

<br>

This is caused by the camera’s inability to create the default folder on the SD card.

If this occurs, complete the following steps:

  1. Remove the SD card and install it into another machine.
  2. Navigate to the SD card’s root.
  3. Create a directory with the name “vadp.”
  4. Reinstall the SD card into the camera and continue with the installation.

<br>

VADP-Upload-Fail-on-Vivotek-Cameras-1.pdf