Description
Drives showing offline or write error on Storage => Drive tab and Hardware tab.

<br>
Workaround
Open Windows device manager (Windows start menu and type “device manager”)
Expand IDE ATA/ATAPI controllers
Check to see if there are duplicate ATA Channel entries (ATA Channel 0, ATA Channel 1, etc)
Disable the “Standard Dual Channel PCI IDE Controller” and reboot to remove the duplicates.
If the “Standard Dual Channel PCI IDE Controller” does not exist, disable the second entry for each duplicate ATA Channel by right clicking and choose disable.
Reboot the server

<br>
Drives-displaying-Red-on-Storage-Drive-and-Hardware-tab.pdf