When using a joystick on Mac-based exacqVision Client software, Z-Axis operations do not work correctly. On an exacqVision Surveillance Keyboard (and most other devices), the joystick’s Z-Axis is mapped to the action of twisting the joystick, which is used to control zoom functions. On some keyboards, zoom functionality can be mapped to a programmable button.… Continue reading Joystick Z-Axis on Mac-based exacqVision Client