Deploying System Lists to Client Users

In large organizations, such as multi-site enterprises, K-12 school districts, or university campuses, some admins will desire the ability to remotely manage the server connections their users have added within their ExacqVision Client application. This can result in faster deployments as well as less user support from their IT/Desktop Support teams, avoiding emailing, printing, or… Continue reading Deploying System Lists to Client Users

Cameras Added With the Wrong Plugin Causes exacqVision Server Crash Loop

Description Adding certain cameras with the wrong plugin type causes the exacqVision Server to go into a crash loop. Product Steps to Reproduce Expected Results Actual Results Solution NOTE:  This has been specifically observed when Illustra cameras are added with Illustraflex instead of Illustra3 and Samsung cameras are added with Onvif instead of Samsung <br>

How to Configure No Close Client Usage

Beginning with version 9.4, the exacqVision Desktop Client offers the ability for administrators to prevent users from deactivating an Event Monitoring profile.  In previous versions, when an Event Monitoring profile was active a user could accidentally deactivate the profile by navigating away from it or by closing the client window. With Client 9.4 or higher,… Continue reading How to Configure No Close Client Usage

Disabling a Drive via XML (Windows)

To disable a drive in a Windows exacqVision Server via XML, complete the following steps: <br> Before editing any configuration files directly, stop your exacqVision Server. Open Control Panel and then the Administrative tools (you might have to select Classic View to see the option).Open the Services link and find exacqVision Server. Right-click and select… Continue reading Disabling a Drive via XML (Windows)