XDV Reference

*** INTERNAL USE *** Type Definitions The options described in the documentation below are listed in dictionary values, where possible. This is indicated by the key values listed between curly braces ‘{ }’. The key is followed by the description of the key value is colon separated, as in the following example:     {key1:description1, key2:description2, …}… Continue reading XDV Reference

Deploying System Lists to Client Users

In large organizations, such as multi-site enterprises, K-12 school districts, or university campuses, some admins will desire the ability to remotely manage the server connections their users have added within their ExacqVision Client application. This can result in faster deployments as well as less user support from their IT/Desktop Support teams, avoiding emailing, printing, or… Continue reading Deploying System Lists to Client Users

How to Configure No Close Client Usage

Beginning with version 9.4, the exacqVision Desktop Client offers the ability for administrators to prevent users from deactivating an Event Monitoring profile.  In previous versions, when an Event Monitoring profile was active a user could accidentally deactivate the profile by navigating away from it or by closing the client window. With Client 9.4 or higher,… Continue reading How to Configure No Close Client Usage