Impact of Microsoft Windows XP End of Support

Microsoft announced the end of support for Windows XP on April 8, 2014. The operating system will no longer receive security updates or technical support after that date.Customers with exacqVision servers running Windows XP will likely have questions about this end of support, and the following information will help answer their questions: Q: Will Exacq upgrade the… Continue reading Impact of Microsoft Windows XP End of Support

Client cannot connect to edvrserver on Windows XP after upgrading edvrserver

Description Client cannot connect to edvrserver on Windows XP after upgrading edvrserver. <br> Introduced Version exacqVision Server 7.7.26+ <br> Fixed Version Not yet fixed <br> Workaround Downgrade edvrserver to a previous version (7.6.x) Since the remote update is not possible, the user has to run an installer on the server manually.

exacqVision Windows XP Support

Microsoft has informed consumers that Windows XP is no longer supported as of April 8, 2014. This means that Microsoft no longer supplies security updates for Windows XP. Note the following information about how this affects exacqVision products. Can I upgrade from Windows XP to Windows 7 on my Exacq-built exacqVision system? Any system built… Continue reading exacqVision Windows XP Support

Enabling 4×3 Resolution to Eliminate Gray Bars in Video Windows (Legacy)

NOTE: These are Legacy instructions. This behavior was replaced when Client settings implemented Panel Size settings.When using cameras with a 4×3 resolution, gray bars might appear to the left and right of the camera’s video window in exacqVision Client. To stretch the 4×3 video so that it fills the screen, manually set the video card… Continue reading Enabling 4×3 Resolution to Eliminate Gray Bars in Video Windows (Legacy)

Assigning a Default Printer to the Windows User (Restricted) Account

If you want to print images from the ExacqVision software on an ExacqVision server, you might need to change the default printer. Because Windows is locked down when you log in as a User, you must perform the following steps to configure the default printer: <br>