Exacq Server is not booting after the windows update reboot.

Description -When updating Windows 10 and rebooting the Exacq unit, it will not come back to boot up again and has to power off manually and power on the unit again on Motherboard “ASRock H110E1” with Firmware version 1.50 Solution The Motherboard BIOS Firmware needs to be updated to version 1.60A The instructions to update… Continue reading Exacq Server is not booting after the windows update reboot.

Windows Updates, Imaging, and LTSx – Information

Description This ticket contains likely KB information for Windows images. First there are wikis here: ​https://trac.exacq.com/DVR/wiki/Windows10InformationandRequirements ​https://trac.exacq.com/DVR/wiki/Windows10DevelopmentEnvironmentCreation ​https://trac.exacq.com/DVR/wiki/Windows10ImageCreation ​https://trac.exacq.com/DVR/wiki/Windows10Verification  The the first wiki is probably of most relevant here. Our image is based on Windows 10 Enterprise 1607 LTSB (Long Term Service Branch)LTSB means the same thing here as it does for ubuntu. It is/was a mature, stable… Continue reading Windows Updates, Imaging, and LTSx – Information

Windows 7 boot issue after MS update

Issue We have had several reports of Windows 7 systems that will no longer boot after installing Microsoft 8/2019 Security update KB4512506. <br> If you have already installed the 8/2019 update release Tuesday 8/13/2019, the windows 7 exacqVision server will no longer boot and you will see the screen below. <br> This also affects Windows… Continue reading Windows 7 boot issue after MS update

Windows update KB3033929 required for 8.6 release

Exacq upgraded they software signing certificate, which means Windows 7 systems will require Windows update KB3033929 for Hardware Monitoring and motherboard watchdog functionality to work. <br> Link to download the KB: https://www.microsoft.com/en-us/download/details.aspx?id=46148 <br>