Description Microsoft provides customers a choose of Server Core or Server with Desktop Experience. Choosing either Microsoft Windows 2019 or 2022 Server Core results in EM being inoperable when installed. Product exacqVision Enterprise ManagerMicrosoft Server 2019 CoreMicrosoft Server 2022 Core Steps to Reproduce Install exacqVision Enterprise Manager on a machine running either Microsoft Windows… Continue reading Installing exacqVision Enterprise Manager on Windows Server Core
Tag: Windows Server
Pelco Motion Notification Could Fail on exacqVision System with Windows Server 2012
A Pelco Pro Sarix camera (IMP-1110) failed to send motion notifications on a Windows Server 2012 system running the the Explicit Congestion Notification (ECN) service. The ECN service and Pelco plugin use the same TCP port 8575; if the ECN starts automatically after system startup, the notification subscription from the Pelco plugin can fail, meaning… Continue reading Pelco Motion Notification Could Fail on exacqVision System with Windows Server 2012
Windows Server & Client and OpenLDAP/Kerberos
The following process allows you to configure exacqVision permissions and privileges for accounts that exist on an OpenLDAP/Kerberos server:1. On the OpenLDAP/Kerberos server, ensure that your installed schema includes the following object types: inetOrgPerson (RFC 2798)organization (RFC 2256)krbPrincipalAux (provided by the Ubuntu krb5-kdc-ldap package) And at least 1 of the following opject types: groupOfNames (rfc… Continue reading Windows Server & Client and OpenLDAP/Kerberos