Internal SATA Drives Show up as Removeable Media

Description In some cases Internal SATA devices (HDDs or SSDs) may show as removable media in your task bar.  Consequently, the safe removal icon appears for the disk in the system tray (as if it is a common USB flash drive). Products Windows 10Windows 7 Enterprise Expected Results The SSD/SATA Drive shows as a Disk… Continue reading Internal SATA Drives Show up as Removeable Media

Windows OS Servers Fail to Correctly Identify Non-DST Time Zones & Prevent Local Client Video Searches from Working

Issue: Servers with Windows operating system (OS) fail to correctly identify non-Daylight-Savings-Time (DST) time zones and prevent the local client searches from working for time periods recorded during DST. Symptoms: Sporadic playback on the server using the (internal) local client and no issues with searching from the (external) client workstations. In other words: search works… Continue reading Windows OS Servers Fail to Correctly Identify Non-DST Time Zones & Prevent Local Client Video Searches from Working