Postgresql will not install with spaces in username

Description The packaged postgresql installer when trying to install ESM, you cannot install it with a username that has spaces. Also, postgresql requires admin to install properly on the machine. You cannot install with a policy group that does not have sys admin on the machine.

exacqVision Installation Fails Because Existing exacqVision Client Instance Remains Open

All instances of exacqVision Client must be closed before successfully upgrading a client installation. The installer normally detects these instances and prompts the user to close them before proceeding. <br> If an exacqVision Client installation is configured to receive VideoPush information from another client, the exacqVision installer will not detect the open client instance. This… Continue reading exacqVision Installation Fails Because Existing exacqVision Client Instance Remains Open