S-Series will not allow configuring volumes via the exacqVision client

If you are configuring your S-Series volumes from the exacqVision client, but they will not initialize, do the following: Check to see if the StorCLI binary is in your path. This is the program that allows exacqVision server to communicate with, and configure drives from the exacqVision client. $ ls /usr/local/bin/storcli If no results are… Continue reading S-Series will not allow configuring volumes via the exacqVision client