Some Samsung models require Motion to be Configured via Cameras Web Interface

Issue Some Samsung models are not supported in regards to motion window configuration.  <br> Workaround  Configure motion windows via the cameras web interface. <br> Resolution Capability added to exacqVision. <br> Version Affected exacqVision Server versions prior to 20.03.123 <br> Version Fixed 20.03.123