Dewarping of Dahua cameras not working on web client or Exacq Mobile 3 (Legacy)

Affected Versions <br> Description In web service 7.6 (Windows only), dewarping of Dahua fisheye cameras does not work. These cameras do not show any dewarping options in the web client or Exacq Mobile 3 app. <br> Workaround <br> Resolution Update exacqVision Web Service to version 8.2.2 or higher <br>

Native Streaming in the Web Client

Affected platforms exacqVision 7.2 or later <br> Description exacqVision 7.2 introduces native h.264 video streaming to the web client. When a browser session connects to the web service, the browser and web service negotiate whether transcoding or native streaming will be used. The following logic describes how this is negotiated: If the browser does not… Continue reading Native Streaming in the Web Client

What type of video does the exacqVision Web Service transmit?

The codec used to transmit video will depending on the plugin used. In many cases the exacqVision Web Service performs transcoding and transmits a compressed JPEG stream of images to the Web Client or Exacq Mobile 3 app. Some plugins are capable of forwarding the H.264 stream without the need to transcode. <br>

How can I find the version of my exacqVision Client, Server, or Web Service software?

exacqVision Server Related links: Download the latest exacqVision Server software <br> exacqVision Client Related links: Download the latest exacqVision Client software <br> exacqVision Web Service Related links:Download the latest exacqVision Web Service <br>