How to: Executing and debugging C# applications with evAPI and Visual Studio 2005 or newer

C# or other managed applications created with Visual Studio 2005 or newer cause a System.AccessViolationException in the EVAPI_CreateWindow function on Windows Vista and Windows 7. To avoid this while debugging within Visual Studio and during application execution, complete the following steps. After the project has loaded, select the project properties under the Project item on… Continue reading How to: Executing and debugging C# applications with evAPI and Visual Studio 2005 or newer