exacqVision Mobile – VideoPush

This feature included in 25H1 improves the collaboration between users of the desktop client and the new exacqVision Mobile app using the VideoPush feature.Chapters:00:00 Intro00:13 Feature Demo00:46 Remote Connections00:56 Configure exacqVision Mobile01:19 Scenario 1 – Sending cameras from Mobile App to Desktop Client01:51 Scenario 2 – Sending cameras from Desktop Client to Mobile App02:28 Scenario… Continue reading exacqVision Mobile – VideoPush

How to Create a Video Wall in exacqVision Using VideoPush

Description  The following instructions and resources can be used to configure a Video Wall using VideoPush in exacqVision. Product  Solution Enable Video Push Video Push must be enabled for each client which will be part of the Video Wall. Layouts If one of the provided templates does not reflect your video wall configuration, use Layouts… Continue reading How to Create a Video Wall in exacqVision Using VideoPush

VideoPush Timeouts

If your client has never been configured as a VideoPush receiver, you will receive a timeout whenever you try to send a VideoPush. As a workaround, select Enable Receiving Display on the Client page on the sending client. You can then disable the option again, if desired. After enabling it at least once, any VideoPush… Continue reading VideoPush Timeouts