*** INTERNAL USE *** Description The psmove utility was designed to move psfiles to the correct location after a time zone change or if a files time does not match frame times. It will perform a search on all local storage drives, read the PSI file header for the start time, determine if the PSI… Continue reading Running psmove on Ubuntu Linux
Tag: Video Files
Copy Video Files While Retaining Modification Date
If the need arises in which you must copy recorded video data from one drive to another it is important to preserve both the file structure and the modification dates of the files. See below for instructions on copying directories to preserve this data: Windows: Using CMD, enter the following: <br> Linux: Using Terminal, enter… Continue reading Copy Video Files While Retaining Modification Date