Special Characters Cause Video Clip to be Removed from Email Notification

Affected VersionsexacqVision 7.6 and priorDescriptionIf a camera name contains characters that are not allowed by the file system on the server’s operating system, the attachment cannot be included in an email notification. The server’s file system prevents the attachment file from being created.WorkaroundIn Windows, the following characters are NOT allowed in the name:Less than symbol [Greater… Continue reading Special Characters Cause Video Clip to be Removed from Email Notification