The validation standard used in ExacqVision is known as HMAC, for Hashed Message Authentication Code, and uses a cryptographic hash and secret cryptographic key. HMAC is used by ExacqVision to verify the integrity of exported video.
The ExacqVision Client software calculates and writes out the message authentication code (MAC) during file export. The ExacqVision ePlayer later calculates a hash and verifies the MAC during authentication using SHA-256. The methodology ensures no alteration of the data as the hashed calculations are compared to be certain the hashes match.
To authenticate video in the ExacqVision ePlayer, select Authenticate from the Tools menu.
The following image shows a successful authentication:
Video may only be authenticated using the ExacqVision ePlayer. The ePlayer application is used to playback ExacqVision native files in .PS or .PSX file formats. It is also packaged in self-playing .EXE file exports. For more information on the features of exported file formats, refer to Article 1894.
<br>