After formatting an SD card for a Vivotek camera, the VADP upload can fail with the following error:
Create “/mnt/auto/CF/vadp” failed
Upload module failed
Upload VADP package failed
<br>
This is caused by the camera’s inability to create the default folder on the SD card.
If this occurs, complete the following steps:
- Remove the SD card and install it into another machine.
- Navigate to the SD card’s root.
- Create a directory with the name “vadp.”
- Reinstall the SD card into the camera and continue with the installation.
<br>
VADP-Upload-Fail-on-Vivotek-Cameras-1.pdf