Installing updates via Terminal The commands are as follows: apt update: Update is used to resynchronize the package index files from their sources on Ubuntu Linux via the Internet.apt upgrade: Upgrade is used to install the newest versions of all packages currently installed on the Ubuntu system. To update software list for Ubuntu First, open… Continue reading Update Ubuntu Linux Software Using Command Line
Tag: Upgrade
How to upgrade LSI firmware
LSI firmware upgrade instructions: Insert the latest Utilities Disk in the system. If that is not available, download the latest driver from here: http://www.avagotech.com/products/server-storage/raid-controllers/megaraid-sas-9271-8i#downloadsBoot into system as adminLaunch MegaRAID Manager (icon on Desktop) and login as adminOn the Dashboard, click on ‘Update Firmware’ under Actions.Select the .rom file in the location r:\Recovery\Drivers\RAID cards\LSI-9271-8i\Firmware (or to… Continue reading How to upgrade LSI firmware
How do I update my exacqVision software?
exacqVision Applications exacqVision software can be thought of as a suite of applications that work together to provide different services. The primary application is the exacqVision Server, which records video, audio, and event data. The exacqVision Client provides an interface to view live and recorded video as well as to configure the server application. A… Continue reading How do I update my exacqVision software?