Updating Apache and Apache Solr on exacqVision Enterprise Manager – Windows

To mitigate currently known vulnerabilities, the following updates are recommended. Apache to 2.4.51, Apache Solr to 7.5.0 and exacqVision Enterprise Manager (EM) to 21.12.1 or higher. Note: Updates for both Apache and Apache Solr are available as part of the EM install package for version 21.09 and higher.  However, updating to EM versions 21.12 or… Continue reading Updating Apache and Apache Solr on exacqVision Enterprise Manager – Windows